How to enable SOE feature at Card Level
Greetings,
i'm using DI880 And DO880 Cards in a project..how to enable SOE feature at Card and how to Verify it. kindly advice.Thanks in advance
i'm using DI880 And DO880 Cards in a project..how to enable SOE feature at Card and how to Verify it. kindly advice.Thanks in advance
Answers
Hi,
Go to Settings in the particular DI or DO SOE card --> Operation Mode Channel 1 --> Select the DI+SOE option in drop down menu this is for card level setting.
Need to connect signalid in the particular SignalInBool block.
Go to Settings in the particular DI or DO SOE card --> Operation Mode Channel 1 --> Select the DI+SOE option in drop down menu this is for card level setting.
Need to connect signalid in the particular SignalInBool block.
Add new comment