Microflex drives "integrated power module failure"
The error was "integrated power module failure" as it flashed twice. It ran for 2 hours then it was flashing constantly meaning power base fault
Answers
If you get an error "10013" then the power module has an error - this can be caused by an over current (spike which is too quick for Firmware to measure) or other internal errors and can normally be cleared by a power cycle. If the problem persists unit might be faulty.
Add new comment