800xA SV5.1 for DSDP 140A with 800M
Hi,
Is anybody know how to Configure DSDP 140A in Control Builder M? We are upgrading MP200 to AC800M(PM866) with module bus CI856. As I notice there is only DSDP 140B in hardware library CI856S100Hwlib. Are these two module the same? When I configure using DSDP 140B in Control Builder it seems the signals not match compare to PC element POS-A (on old MP200 PC Program). The variable input in POS-A seems to become variable output in DSDP 140B hardware connection (CBM).
Best Regards,
Hansen
Is anybody know how to Configure DSDP 140A in Control Builder M? We are upgrading MP200 to AC800M(PM866) with module bus CI856. As I notice there is only DSDP 140B in hardware library CI856S100Hwlib. Are these two module the same? When I configure using DSDP 140B in Control Builder it seems the signals not match compare to PC element POS-A (on old MP200 PC Program). The variable input in POS-A seems to become variable output in DSDP 140B hardware connection (CBM).
Best Regards,
Hansen
Answers
Not all S100 Board Types are supported with CI856. If DSDP140A is not available, you may want to cross-check with Documentation and ask your ABB support contact for options.
DSDP140A is not mentioned in the list of supported modules for 800xA 5.1
See manual 3BSE038018-510 H for details
Best Regards
Jan-Erik
See manual 3BSE038018-510 H for details
Best Regards
Jan-Erik
Add new comment