ACS800-104-0580-7 CURRENT UNBALANCE 2330 AFTER CURRENT REACH 440A OF INU UNIT PLS GUIDE THE PROPER SOLUTION ???
Answers
Hi
a problem of imbalance in the phases can be caused by multiple factors and I do not believe the solution lies in some programming parameter, also because I imagine that until some time ago, the problem did not arise. I suggest you contact the nearest ABB service that can help you resolve this fault.
BR
Flavio
a problem of imbalance in the phases can be caused by multiple factors and I do not believe the solution lies in some programming parameter, also because I imagine that until some time ago, the problem did not arise. I suggest you contact the nearest ABB service that can help you resolve this fault.
BR
Flavio
Add new comment