node ip address wrong
Hello
We have one 800XA 5.1 rev E version.-
and have redundant aspect server.
The physycal address of one of the server is 172.16.4.1. that correspond to PRIDCAS1
![]()
BUT SERVICES IN THIS ASPECT server ARE NOT RUNNING BECAUSE APPEARS WRONG IP ADRESS: 172.16.4.200 in the configuration
HOW IS IT POSSIBLE TO REVERT IP ADDRESS TO THE RIGHT IN configuration? please see the image below
Thanks for any sugestion.

We have one 800XA 5.1 rev E version.-
and have redundant aspect server.
The physycal address of one of the server is 172.16.4.1. that correspond to PRIDCAS1
BUT SERVICES IN THIS ASPECT server ARE NOT RUNNING BECAUSE APPEARS WRONG IP ADRESS: 172.16.4.200 in the configuration
HOW IS IT POSSIBLE TO REVERT IP ADDRESS TO THE RIGHT IN configuration? please see the image below
Thanks for any sugestion.
Answers
Check:
Be aware of: the aspect shown in the image has a lesser known feature; remote nodes are listed with DNS\hosts info while the own node is listed with the local network adapter settings.
- The DNS forward zone
- %systemroot%\system32\drivers\etc\hosts file
- RNRP Monitor
Be aware of: the aspect shown in the image has a lesser known feature; remote nodes are listed with DNS\hosts info while the own node is listed with the local network adapter settings.
Add new comment