A5001 fault code in ABB ACS355 drive
Answers
Hi
directly from the ACS355 FW manual:
5001 - Drive is not responding - Check panel connection.
This can mean that you have a problem on the interface of the communication panel - drive side. If you have other units, again from ACS355, you can try swapping the panel. If the problem persists even on another drive, you will have to change the panel. If the problem no longer occurs, you will probably have to change the drive because the repair is not convenient.
Hope this help you
BR
Flavio
directly from the ACS355 FW manual:
5001 - Drive is not responding - Check panel connection.
This can mean that you have a problem on the interface of the communication panel - drive side. If you have other units, again from ACS355, you can try swapping the panel. If the problem persists even on another drive, you will have to change the panel. If the problem no longer occurs, you will probably have to change the drive because the repair is not convenient.
Hope this help you
BR
Flavio
Source: ACS355 FW Manual
Did you fix the a5001 error ?
ihave the same one
please help
Add new comment