AFW time service for non 800xA nodes
Is there any way to use afwtimeservice for non 800xa nodes ?
If afwservice can be installed to non 800xa nodes without installing compleate 800xa package - like RNRP is installed when we are deploying node as generic node
If afwservice can be installed to non 800xa nodes without installing compleate 800xa package - like RNRP is installed when we are deploying node as generic node
Answers
No, you must use other functions, like e.g. Win32Time.
Hello,
Only nodes (part of Node admin str-other than pseudo nodes) which runs with 800xA core software supports afw time service.
If you want to run configure time sync in other non-xA nodes like Domain/utility nodes can be sync by using SNTP like ex:
Ensure W32time is running in non-xA nodes to use SNTP to work.
Only nodes (part of Node admin str-other than pseudo nodes) which runs with 800xA core software supports afw time service.
If you want to run configure time sync in other non-xA nodes like Domain/utility nodes can be sync by using SNTP like ex:
- Configure Domain (PDC) as SNTP client and server to get time from GPS via RNRP router or directly based on the GPS Connection on your network.
- Configure other domain clients as NTP clients to get sync from PDC so that PDC will advertise time to NTP clients.
Ensure W32time is running in non-xA nodes to use SNTP to work.
Add new comment