Falta Error on Online Builder
Voted best answer
On-Line Builder can be used only for programming of AC450, AC410, MP200 controllers and for RTA board configuration.
Different procedure is used to get in AC160 online. AC160 can be connected on-line through Function Chart Builder using serial COM port.
In the Upper menu there is option Target Connect.
Different procedure is used to get in AC160 online. AC160 can be connected on-line through Function Chart Builder using serial COM port.
In the Upper menu there is option Target Connect.
Answers
Good day;
I realized what the customer was done when he get the mentionated error. The error appear whent he try con connect one of the CBA Engineering Client station to an AC450 controller using the RTA connected a one CBA Engeneering Server Station but the RTA is already used. The servers of the system are virtualiced the customer was confused about how to use the system to enginering task in the controllers.
Regards
I realized what the customer was done when he get the mentionated error. The error appear whent he try con connect one of the CBA Engineering Client station to an AC450 controller using the RTA connected a one CBA Engeneering Server Station but the RTA is already used. The servers of the system are virtualiced the customer was confused about how to use the system to enginering task in the controllers.
Regards
Add new comment