Implementation of 800xA system mutisystem integration between two diffrent 800xA system through firewall.
Hi guys,
Need one information we are integrating two diffrent 800xA system via multisystem integration located in two diffrent areas. The IP series of two different 800xA systems is start with as per our standard 172.16.0.0, the two 800xA systems are connecting via through firewall. Our 800xA system IP's translating from 172.16.0.0 series to 10.101.40.0 Via firewall at one end of 800xA system (Data provider). At the other end we are translating again from 10.101.30.0 to 172.16.0.0 via firewall at another end of 800xA system(Data subscriber).
so in this case i need one clarification of ports which needs to be open in firewall, I have checked in multisystem manual is mentioned that 3340 port is for multisystem integration , is that only port is enough for getting data from Data provider 800xA system to Data subscriber 800xA system as per this configuation or any other ports needs to be allowed or any other things to be taken care.. sample Configuration is attached. I really want information about Ports which are allowed for MSI apart from 3340 port.. kindly suggest , thanks
Note : 10.101.**.** is plant corporate network. Via plant corporate network we are doing multisystem integration using firewalls.
Need one information we are integrating two diffrent 800xA system via multisystem integration located in two diffrent areas. The IP series of two different 800xA systems is start with as per our standard 172.16.0.0, the two 800xA systems are connecting via through firewall. Our 800xA system IP's translating from 172.16.0.0 series to 10.101.40.0 Via firewall at one end of 800xA system (Data provider). At the other end we are translating again from 10.101.30.0 to 172.16.0.0 via firewall at another end of 800xA system(Data subscriber).
so in this case i need one clarification of ports which needs to be open in firewall, I have checked in multisystem manual is mentioned that 3340 port is for multisystem integration , is that only port is enough for getting data from Data provider 800xA system to Data subscriber 800xA system as per this configuation or any other ports needs to be allowed or any other things to be taken care.. sample Configuration is attached. I really want information about Ports which are allowed for MSI apart from 3340 port.. kindly suggest , thanks
Note : 10.101.**.** is plant corporate network. Via plant corporate network we are doing multisystem integration using firewalls.
Answers
Only TCP 3340 (or any other available port as it can be chosen almost arbitrarily) needs to be opened.
Below an image of TCPview.exe (from www.sysinternals.com) when run on an MI Remote Access Server.
I have marked remotely connecting MI Remote Access Client subscribers yellow.

Below an image of TCPview.exe (from www.sysinternals.com) when run on an MI Remote Access Server.
I have marked remotely connecting MI Remote Access Client subscribers yellow.

Add new comment