Install of updated Freelance IO license gives error denying write access to the registry key ?
See comment from customer :
"We have just received a updated IO Licence key for Freelance (following recent additions)
I have installed the key (When I click on Install - it says successfully).
Then when I click on the OK....it gives the following message denying write access to the registry key. (See attached)
I have tried this logged on to the Engineering Station as OperateITService, 800XAService and 800XAInstaller, and get the same response.
Freelance still shows 10900 IO, where the code in the new key shows 11500"
Add new comment