Remote I/O Interface / Remote I/O Definition Block Order in Harmony
FC 146 is required to have a lower block number than its FC 147 blocks and the slaves it handles.
40% of the sites checked did not have the FC 146 block at the lowest block number. Enough of these also were checked to be satisfied that those situations are not ones where auto-sequencing is enabled.
Can anyone explain what does not work properly if the blocks are not in the required order? We can detect this and give a warning message, but we should know that there is a real problem other than a one scan lag.
Thanks.
40% of the sites checked did not have the FC 146 block at the lowest block number. Enough of these also were checked to be satisfied that those situations are not ones where auto-sequencing is enabled.
Can anyone explain what does not work properly if the blocks are not in the required order? We can detect this and give a warning message, but we should know that there is a real problem other than a one scan lag.
Thanks.
Answers
This question has not yet been answered.
Add new comment