ACS355-01E and ACS355-03E
Hi,
I have ACS355-03E-02A4-2 driver.
Can I use single phase supply power up the driver?
Thank in advance
I have ACS355-03E-02A4-2 driver.
Can I use single phase supply power up the driver?
Thank in advance
Voted best answer
Hi
you can try powering the drive with 220 V single-phase, but you have to be careful that the final current from the drive might not be the nominal one, because you only have two input phases and not three.
BR
Flavio
you can try powering the drive with 220 V single-phase, but you have to be careful that the final current from the drive might not be the nominal one, because you only have two input phases and not three.
BR
Flavio
Add new comment