Smart Client Trend positioning
Hi guys,
I've added six trend windows on one panel (Smart Client connected to 800xA v5.1). When I open the Smart Client application, those trends aren't evenly distributed across the panel. So every time after reopening the Smart Client Application I have to manually resize/position those trends across the panel. Is there an option/property to fix those trends to be distributed/positioned evenly across the panel (picture in the attachment).
Thanks in advance,
Hrvoje
I've added six trend windows on one panel (Smart Client connected to 800xA v5.1). When I open the Smart Client application, those trends aren't evenly distributed across the panel. So every time after reopening the Smart Client Application I have to manually resize/position those trends across the panel. Is there an option/property to fix those trends to be distributed/positioned evenly across the panel (picture in the attachment).
Thanks in advance,
Hrvoje
Voted best answer
We have done some experimentation with this question, and attached you will note some of the findings. Note also that this is assuming that the Panel is utilizing a Native Smart Client Panel, as imported PG2 Trend displays do not have the capability to enter into the Design Mode of Smart Client for editing purposes. Additional capabilities exist that allow for the editing of parameters within the actual PXL file that is created, as all the parameters of the Panel are available when reading this file into an application such as Notepad. Any questions you may have concerning these examples will be answered if possible.
Please be aware that this testing was done on the most recent version of Smart Client, ver. 2.2 RevD.
Regards,
Geof
Please be aware that this testing was done on the most recent version of Smart Client, ver. 2.2 RevD.
Regards,
Geof
Add new comment