How do you sync the Faceplate colors are different on the client than Symphony Plus Operations Server?
In Symphony Plus 2.1.2, the system was reloaded. The SPO clients have the same graphics and tags but the faceplate controls popups are showing different colors that the server and previous system? Is the BLCOLdeck.xml controlling the colors on the client or is it in the registry?
These are custom Faceplates for Stations with additional arrows for ramping than the standard faceplates. The server shows the correct colors as the previous version also.
Any thoughts would be helpful.
These pertain to:
FACEPLATE PRCTRL.pop_harm_analog PRCTRL.pop_harm_digital PRCTRL.pop_harm_msdd PRCTRL.pop_harm_rcm PRCTRL.pop_harm_rmsc PRCTRL.pop_harm_station PRCTRL.pop_harm_station_witharrows
These are custom Faceplates for Stations with additional arrows for ramping than the standard faceplates. The server shows the correct colors as the previous version also.
Any thoughts would be helpful.
These pertain to:
FACEPLATE PRCTRL.pop_harm_analog PRCTRL.pop_harm_digital PRCTRL.pop_harm_msdd PRCTRL.pop_harm_rcm PRCTRL.pop_harm_rmsc PRCTRL.pop_harm_station PRCTRL.pop_harm_station_witharrows
Answers
Dear Dan,
runtime the S+ Operations SW uses the registry to read the logical color configuration, there's a mechanism to update client registry from server but maybe it didn't work. You should be able to fix the issue by exporting the registry in the server side (folder ..APPS\LogicalColors) and import them on the client size in the same registry folder.
Hope this will fix your issue.
Mauro
runtime the S+ Operations SW uses the registry to read the logical color configuration, there's a mechanism to update client registry from server but maybe it didn't work. You should be able to fix the issue by exporting the registry in the server side (folder ..APPS\LogicalColors) and import them on the client size in the same registry folder.
Hope this will fix your issue.
Mauro
Add new comment