800xA shared variable issue
We have found a problem with the shared variables in PG2. It's possible to write to a shared variable and obtain different value in each instance. Is there a fix for this problem in 6.0.3. To replicate this, you can create a symbol that is writing _now#millisecond to a variable that is local and another that is shared. You create an event «On Create» that execute this write. You create 2 instances of this symbol in a graphic. You will see that the shared variable in symbol 1 is equal to local variable of symbol 2 and the same shared variable in Symbol 2 is equal to symbol 1 local variable. The shared variable get synchronized again after any write to it.
Answers
Have you installed rolup 5 for the base system? It contains fixes for shared variables not updating.
by Stefan Stromqvist
I believe you should ask your regional Support Center for a correction while posting here on the forum for a workaround for your issue.
by Steve Berteau BBA Rank: 209 on 10/29/2019 6:31:47 AM | Like (0) | Report
I don’t want to provide an SID charge number when it’s an 800xA problem.
Add new comment