800xA Multi node Installation on Azure VM
Hi,
I have two Azure VM, Server 1 & 2. I have setup the Azure virtual network , so both servers are in same network only and pings each other.
Server OS: Windows 2016 server
800xA Version : 6.1
Server1 : 172.16.4.11 255.255.252.0
Server2 : 172.16.4.12 255.255.252.0
I have installed 800xA base on both server. The problems are
1. I can't able to add node Server2 from SCC in Server1
2. I can't see server 2 in RNRP Status tool.
3. Is it possible to do the multi node installation on Azure ?
4. Azure says that it won't support multicast. I hope RNRP requires free multicasting.
Please provide solution and if more info needed, I will do.
Thanks in Advance.
I have two Azure VM, Server 1 & 2. I have setup the Azure virtual network , so both servers are in same network only and pings each other.
Server OS: Windows 2016 server
800xA Version : 6.1
Server1 : 172.16.4.11 255.255.252.0
Server2 : 172.16.4.12 255.255.252.0
I have installed 800xA base on both server. The problems are
1. I can't able to add node Server2 from SCC in Server1
2. I can't see server 2 in RNRP Status tool.
3. Is it possible to do the multi node installation on Azure ?
4. Azure says that it won't support multicast. I hope RNRP requires free multicasting.
Please provide solution and if more info needed, I will do.
Thanks in Advance.
Answers
800xA require RNRP
RNRP require IP multicasting
Azure does not allow IP multicasting.
Please contact your regional ABB sales representative; solutions to the above is underway, but not yet released.
RNRP require IP multicasting
Azure does not allow IP multicasting.
Please contact your regional ABB sales representative; solutions to the above is underway, but not yet released.
Add new comment