Aspect server using server grade & Connectivity server using workstation grade
Hi All
Existing system is using 800xA 6.0 version and using workstation grade as ASCS (combine). As per question,we would like to propose the Aspect server using server grade (windows server) & Connectivity server using workstation grade (windows 10 LTSB). Is it posibble? any limitation?
Existing system is using 800xA 6.0 version and using workstation grade as ASCS (combine). As per question,we would like to propose the Aspect server using server grade (windows server) & Connectivity server using workstation grade (windows 10 LTSB). Is it posibble? any limitation?
Answers
Refer to System Guide, all options are described there. You can mix server and workstation but redundant functions should use the same Operating System.
If you run Connectivity Server (or any other Server function) on Windows 10, your System Size is limited to max. 16 Nodes
If you run Connectivity Server (or any other Server function) on Windows 10, your System Size is limited to max. 16 Nodes
Add new comment