Communication of REF542pluse with USB to RS232 DB9 serial port adapter cable
Voted best answer
Hi,
The HMI must be interfaced to a PC through the ABB RS232 optical cable. The optical converter must be plugged in the connector situated on the front side of the HMI. By using this interface the configuration file can be downloaded or uploaded from the local PC, which hosts the configuration tool, to the REF542plus central unit.
BR
ATP
The HMI must be interfaced to a PC through the ABB RS232 optical cable. The optical converter must be plugged in the connector situated on the front side of the HMI. By using this interface the configuration file can be downloaded or uploaded from the local PC, which hosts the configuration tool, to the REF542plus central unit.
BR
ATP
Answers
Hi
you should kindly specify with which series of ABB drives you want to try to connect with the device you have described ... there are many series and different types of ways to communicate.
If you give us more and detailed information, we can help you better
BR
Flavio
you should kindly specify with which series of ABB drives you want to try to connect with the device you have described ... there are many series and different types of ways to communicate.
If you give us more and detailed information, we can help you better
BR
Flavio
Add new comment