On Symphony Plus Operations v2.1sp2, how does the symbol and graphic replication work to the clients?
In the 2VAA001149-212_B_en_Splus_Operations_2.1_SP2_Display_builder_user_manual.pdf, I see the Graphic Builder section for "Network Distribution Class" for graphics but is the symbols distributed the same way? Is the "Remove From System" only for the local file structure and not the redundant servers?
Answers
"Network Distribution Class" is required at graphic page level only for deployment purpose. The symbols are used inside the graphic files. So NDC at symbols is not required. Similarly, the "Remove to System" is for local server level (Graphic pages) only and not for any remote machines.
Add new comment