ABB Freelance 2016 SP1 Communication Problem
Dear Sir
i am working with Freelance 2016 Sp1. In this Project Controller Using PM902F With Redundancy Application. Here Master Communication Module is CI930F. AS i said before its a Redundancy application, so My first Controller (Primary PM902F) Display is Not ON as its PWR Indication Showing Green LED,Also CI930F is also in OFF Position. Here I Lost My communication with Controller, When i Try to do PING The IP Address of the Controller Primary Controller( IP :172.16.1.10) Its showing Destination Host Unreachable. Already i had checked Hardware side wiring its ok. Could Some one tell me what is the exact problem to lost communication.
For reference Purpose i am attaching the Screenshots Below
i am working with Freelance 2016 Sp1. In this Project Controller Using PM902F With Redundancy Application. Here Master Communication Module is CI930F. AS i said before its a Redundancy application, so My first Controller (Primary PM902F) Display is Not ON as its PWR Indication Showing Green LED,Also CI930F is also in OFF Position. Here I Lost My communication with Controller, When i Try to do PING The IP Address of the Controller Primary Controller( IP :172.16.1.10) Its showing Destination Host Unreachable. Already i had checked Hardware side wiring its ok. Could Some one tell me what is the exact problem to lost communication.
For reference Purpose i am attaching the Screenshots Below
Answers
What led's are lit on the controller?
On the photo it looks like:
PWR led green
ERR Red
RUN off
P/S off
Batt off
Display blank
How does the secondary controller look?
On the photo it looks like:
PWR led green
ERR Red
RUN off
P/S off
Batt off
Display blank
How does the secondary controller look?
Add new comment