Problems running installation 6.0.3.2
I have several clients in our system running Win10 in our domain. Trying to install 800xA 6.0.3.2 there are some of them where the installation works fine and there are some of them where it doesn’t. The problems is during NPT and it looks the same. The virtual clients are made from the same template.
Answers
Hi!
Please observe Win 10 versions for version 6.0.3.2:
Windows 10 IoT 2015 LTSB, Windows 10 Enterprise 2015 LTSB, Windows 10 IoT 2016 LTSB and Windows 10 Enterprise 2016 LTSB.
Regards
Hi.
I had the same error; just you most to wait and run the NPT 10 minutes later the node start. This error appear because the node is not finished the start procedure.
Regard
I had the same error; just you most to wait and run the NPT 10 minutes later the node start. This error appear because the node is not finished the start procedure.
Regard
Add new comment