800xA Operator Workplace resolution problems
Hello,
we are trying to configure three screen operator workplace with different screen resolutions (two screens 1920x1200 and one 4K screen) and are unable to do so. We have only one PG2 Graphic Display to be shown on 4k screen and that one have 4k resolution. Windows Title Bar is displayed in good resolution but PG2 display is pixelated. Do you have any idea how to fix this?
Besides resolution we are facing problems with ABB Clock. Clock is displayed as a part of Operator Workplace Application bar. If Operator Workplace is started from Server, Clock is displayed as it should be, but when started from Client node Clock is in italic. How could we fix this?
thanks in advance !
Lucija
we are trying to configure three screen operator workplace with different screen resolutions (two screens 1920x1200 and one 4K screen) and are unable to do so. We have only one PG2 Graphic Display to be shown on 4k screen and that one have 4k resolution. Windows Title Bar is displayed in good resolution but PG2 display is pixelated. Do you have any idea how to fix this?
Besides resolution we are facing problems with ABB Clock. Clock is displayed as a part of Operator Workplace Application bar. If Operator Workplace is started from Server, Clock is displayed as it should be, but when started from Client node Clock is in italic. How could we fix this?
thanks in advance !
Lucija
Answers
> " three screen operator workplace with different screen resolutions (two screens 1920x1200 and one 4K screen)"
Don't. Many programs can have issues doing this - not just 800xA. Life will be much easier if you configure all monitors to the same resolution.
Don't. Many programs can have issues doing this - not just 800xA. Life will be much easier if you configure all monitors to the same resolution.
Are you using the large view class ?
You can add a view class mapping aspect in your workplace.
Then, you specify that graphic display pg2 and faceplate pg2 should use the large one.
You can add a view class mapping aspect in your workplace.
Then, you specify that graphic display pg2 and faceplate pg2 should use the large one.
Add new comment