Use of the designation aspect in the alarm list?
Hello,
in the system documentation "3BSE041389-510_en_System_800xA_5.1_System_Planning" 3 aspects are described to create a kind of plant hierarchy. They are called designation aspects with name and description.
In the user structure --> My Computer Profile Values --> Name Composer, I can change the Compose string property.
If I set this to ARD (absolutely referenced target), then I see the following entry in 800xA
Is it possible to display this path (ARD) in the alarm list? Or is it possible to read this path and e.g. display it in a graphic object?
Which settings have to be made?
thanks in advance,
Stephan
Voted best answer
This is really not my cup of tea, rather some old legacy of the Function Designer. As per the text in the user's guide I believe only the aspect browser of the Plant Explorer/Engineering workplaces will be affected.

I believe the alarm and event lists display regular (relative) names due to the very restricted amount of space available there.

I believe the alarm and event lists display regular (relative) names due to the very restricted amount of space available there.
Add new comment