ACS800 Drive with NEW AINT-02C
We have ACS800 Drive.
ACS800-04-0400-3+D150
600 Amp Output
we have problem with AINT-02 C.
we have received New card and fitted. Started drive motor is running smoothly.
but we noticed on AINP-01C card Green Led is Off.
before we replace the new AINT it used to remain ON
with New AINT it is relain Off. Also noticed one Power resistor of value 4 Ohm getting very hot.
we have switched off the drive.
Do we need to transfer any parameter etc in New AINT-02C card ?
why AINP-01C Green Led is off.
can we run the drive ??
Answers
This question has not yet been answered.
Add new comment