PP877/ AC800M - Softcontroller Testing
Hello
Is it possible to simulate both process panel (PP877) in simulator mode and AC800M in softcontroller and intereconnect these two for testing.
Mode of Communication is Control Network - MMS .
Is it possible to simulate both process panel (PP877) in simulator mode and AC800M in softcontroller and intereconnect these two for testing.
Mode of Communication is Control Network - MMS .
Answers
Yes, you can, but they can not be on same computer.
If you have Panel Builder (PB) and Compact Control Builder (CCB) on one PC, and then run the SoftController on a seconds PC, then it works.
Start a Virtual PC (or two) on you computer. In one of them you can start SoftController(s) and in the other (or if you run on the host) you run CCB and PB and you can run the Panel Builder application in 30 minutes with the MMS traffic.
by kstoilov
Hi,
Unfortunately I have never tested such. Have a look in the answer below - it could help you
Add new comment