Missing Properties in 'Control Module 'aspect after backup Import
While trying to bring a new library from SV5.1 FP4 rev D system to SV5.1 FP4 Rev E , facing problem after import with few control module types .
The 'Property view' tab in the imported Control Module Type 'Control Modules aspect is blank in Engineering Workplace. though the parameters and variables are imported properly in the control Builder.
Getting a warning message for the modules with such behaviour while import ' Skipped aspect 'Control Module Types Reference 'because of missing Aspect Category 'Control Module Types'
Answers
Did the import process completed without any errors/warnings. Did you export the library using "export library" button or directly dragged/dropped in import/export tool? Adding some screen shots with question wouldn't hurt.
Add new comment