back up system configuration
Is there system 800xa configuration console available in industrial it 800 xa 5.0 sp1 (5.0.1) ? I can't find any tool for automatically back up system data periodically.
Answers
Im not 100% sure, but I think the best way to handle backups and schedule backups is via the plant explorer workplace
You have to configure Backup service in Service Structure. In maintenance structure you have to configure a backup object. Finally you will have to create a schedule task that will start your backup according to the specified period in 800xA
Hello,
xA5.0 Doesn't have system configuration console.
You have to configure manually under the scheduling str but administering/managing old backups to be done from service str-backup service
xA5.0 Doesn't have system configuration console.
You have to configure manually under the scheduling str but administering/managing old backups to be done from service str-backup service
I think the best way is to configure Backup service in Service Structure.
google street view
google street view
Add new comment