GPI04 - Can I download added points to a GPI file on-line?
I have added some new points to a GPI04 file. I am downloading to a pair of redundant MFP02 modules. Can I download the new GPI file on-line or does it have to be off-line if new points are added?
Voted best answer
Hi Linda,
Assuming that we are talking about Symphony Plus GPI V4.0. Changes to the GPI configuration can be done online as per the procedure in the user guide (3BCA010145R1701). The behavior of the GPI component of the configuration during online change is slightly different to the function block component, it's not major but needs to be appreciated. For additions I would ensure that any new function blocks required are installed before the change to the GPI configuration is made.
Good luck,
Alan
Assuming that we are talking about Symphony Plus GPI V4.0. Changes to the GPI configuration can be done online as per the procedure in the user guide (3BCA010145R1701). The behavior of the GPI component of the configuration during online change is slightly different to the function block component, it's not major but needs to be appreciated. For additions I would ensure that any new function blocks required are installed before the change to the GPI configuration is made.
Good luck,
Alan
Source: 3BCA010145R1701
Add new comment