ERROR CI867 HARDWARE LIBRARY
Hi Expert,
I've project with modbus card CI867, so we use firmwire 5.1.2403 with hardware library "CI867Modbus TCPHWLIB 2.3.-3", we want to downgrade the
hardware library to "CI867Modbus TCPHWLIB 1.1-72", but we found some error when we tried to download
ERROR 9096, “The Communication Protocol in Connected library for CI867 at position 3 Invalid”. Why this error pop up? I use the same hardware lib for modbus just different version?
I've project with modbus card CI867, so we use firmwire 5.1.2403 with hardware library "CI867Modbus TCPHWLIB 2.3.-3", we want to downgrade the
hardware library to "CI867Modbus TCPHWLIB 1.1-72", but we found some error when we tried to download
ERROR 9096, “The Communication Protocol in Connected library for CI867 at position 3 Invalid”. Why this error pop up? I use the same hardware lib for modbus just different version?
Answers
Greetings,
There are 2 different type of CI867 HW Libraries exist.
If you want to use Version 1.1.xx, then you need to install sutable hardware library.
Please see attached file.
Hope it helps you.
There are 2 different type of CI867 HW Libraries exist.
If you want to use Version 1.1.xx, then you need to install sutable hardware library.
Please see attached file.
Hope it helps you.
by ATP
avoid duplicating the questions
Add new comment