I'm connecting Areva P139 to RTU560 (CMU02) using IEC103, Status (DPI), Control (DCO) & local/remote not working
I'm connecting Areva P139 relay to RTU560 (CMU02) using IEC103, connection to the relay is established & SPI & AMI signals are updating but for Status (DPI) & Control (DCO) is not working. In relay database Type ID for Breaker, Disconnector & Earth switch status is mentioned as 68, Type ID for Breaker, Disconnector & Earth switch control is 13 & Type ID for Local/Remote is 72.
In RTU the supported Type ID for Status is 1 (SPI/DPI) & Type ID for Control is 20.
I even tried to do the monitoring between RTU & Relay. Relay is sending the Breaker status with Type ID 68, function no 242 & information no is 1 but in RTU it shows in Invalid(IV) & same for local/remote relay is sending with type ID 72, function no 248 & information no 112.
Here i've attached the relevant snap shot for IEC103 sniffing, relay database & RTU sub-device IEC103 document.
the RTU firmware we are using is 12.4.8
kindly help me to solve this issue.
In RTU the supported Type ID for Status is 1 (SPI/DPI) & Type ID for Control is 20.
I even tried to do the monitoring between RTU & Relay. Relay is sending the Breaker status with Type ID 68, function no 242 & information no is 1 but in RTU it shows in Invalid(IV) & same for local/remote relay is sending with type ID 72, function no 248 & information no 112.
Here i've attached the relevant snap shot for IEC103 sniffing, relay database & RTU sub-device IEC103 document.
the RTU firmware we are using is 12.4.8
kindly help me to solve this issue.
Answers
This question has not yet been answered.
Add new comment