800xA Workplace display issue.
Hi Friends,
We have to configure a 4 screen workplace on a single OWS and 4 large screens with resolution 1920x1080.
Once we have configured it and launch it it is unable to detect Individual LCD for Individual display.
and the displays are somewhat distributed in between screens(half on one screen and half on the other.
We are unable to make it full screen.
However once we are logged in via Service account we can launch 4 workplaces and manually place them on screens.
Can any one point out where are we making mistake.
We are working on 800xA 6.0.3
Thanks and regards
Mustafa Z
We have to configure a 4 screen workplace on a single OWS and 4 large screens with resolution 1920x1080.
Once we have configured it and launch it it is unable to detect Individual LCD for Individual display.
and the displays are somewhat distributed in between screens(half on one screen and half on the other.
We are unable to make it full screen.
However once we are logged in via Service account we can launch 4 workplaces and manually place them on screens.
Can any one point out where are we making mistake.
We are working on 800xA 6.0.3
Thanks and regards
Mustafa Z
Answers
Hi,
I could recommend you to read the manual 3BSE030322-600 Operator Workplace Configuration.
There is a special section for configuring of Multiple Screens.
In case you can handle displays in service mode, most probably you have to configure operator workplace and multiple screens in 800xA.
I could recommend you to read the manual 3BSE030322-600 Operator Workplace Configuration.
There is a special section for configuring of Multiple Screens.
In case you can handle displays in service mode, most probably you have to configure operator workplace and multiple screens in 800xA.
Source: 3BSE030322-600
by Sa2016 Rank: 587 on 10/8/2020 8:56:46 AM | Like (0) | Report
Hi, Please let me know how did you fix this issue, I have a similar issue..
Add new comment