REDUNDANCY IMPOSSIBLE AC900F
Hi
I have two controller AC900F with different adress ip in ETH1 (172.16.1.1 and 172.16.1.2) in the two controller i'm activated the eth2 with the standard ip but when i'm plug the RJ45 one the both controller one of them stay in bootloader waiting.
When i'm unplug the RJ45 in eth2 and restart the two controller every controllers works fine independately.
Thank you
I have two controller AC900F with different adress ip in ETH1 (172.16.1.1 and 172.16.1.2) in the two controller i'm activated the eth2 with the standard ip but when i'm plug the RJ45 one the both controller one of them stay in bootloader waiting.
When i'm unplug the RJ45 in eth2 and restart the two controller every controllers works fine independately.
Thank you
Answers
Greetings,
I guess you forgot to define ETH2 as Redundancy Link.
Please see below link for Redundancy Confguration of AC900F:
https://forum-controlsystems.abb.com/...
Hope it helps.
I guess you forgot to define ETH2 as Redundancy Link.
Please see below link for Redundancy Confguration of AC900F:
https://forum-controlsystems.abb.com/...
Hope it helps.
Add new comment