How can I install MMS/OPC Server with RNRP in a Windows 8.1 32-bits Operating System?
Hello,
We need to install MMS/OPC server with RNRP in a Windows 8.1 32-bits Operating System.
We could install CCB 5.1.0 and could communicate with the controller, but we can't install RNRP driver. I get a message that it does support up to Windows 7, and the installer closes.
Do we need to use an older version? or a newer?
There is some workaround to get it running?
Thank you, in advance!,
Best regards,
We need to install MMS/OPC server with RNRP in a Windows 8.1 32-bits Operating System.
We could install CCB 5.1.0 and could communicate with the controller, but we can't install RNRP driver. I get a message that it does support up to Windows 7, and the installer closes.
Do we need to use an older version? or a newer?
There is some workaround to get it running?
Thank you, in advance!,
Best regards,
Voted best answer
Try with RNRP from some CCB or 800xA v6 media, e.g. 6.0 was released when Windows 8 was the main stream client OS.
Add new comment