Possibilities for usage of the location destination aspect
Hello
in location structure I can add a location destination aspect. Is the location destination only visible in location structure? Or is possible to use the location destination in alarm list or in faceplate. Maybe there is some manual existing ;-)
Thanks!
Greetings Stephan
in location structure I can add a location destination aspect. Is the location destination only visible in location structure? Or is possible to use the location destination in alarm list or in faceplate. Maybe there is some manual existing ;-)
Thanks!
Greetings Stephan
Answers
An object starts off with one structure aspect, also called insertion point, eg ”Control Structure”.
By using the Insert Object... command additional structure aspects are added to the same object. Now you have one (1) object with two (2) insertion points or ”legs”.
There is no limit on number of ”legs”, study the root object it has 6 or 7 from start.
An object is deleted from the system when the last ”leg” is removed.
By using the Insert Object... command additional structure aspects are added to the same object. Now you have one (1) object with two (2) insertion points or ”legs”.
There is no limit on number of ”legs”, study the root object it has 6 or 7 from start.
An object is deleted from the system when the last ”leg” is removed.
Every Aspect is visible in every Structure (that the object is inserted in to)
Add new comment