PG2 Drag Handle Input Method Question
Hello,
I dont have too much experience working with operator workplace screen design. I am implementing a virtual Lever to control the movements of a reclaimer and now facing some problems using the drag handle input method.
The behaviour of the horizontal movements (Direction property) is different of the vertical ones. After certain amount of time in determined position, the screen element (with horizontal direction configured) is returning to the zero position.
Have someone faced this kind of problem?
Best regards,
I dont have too much experience working with operator workplace screen design. I am implementing a virtual Lever to control the movements of a reclaimer and now facing some problems using the drag handle input method.
The behaviour of the horizontal movements (Direction property) is different of the vertical ones. After certain amount of time in determined position, the screen element (with horizontal direction configured) is returning to the zero position.
Have someone faced this kind of problem?
Best regards,
Answers
This question has not yet been answered.
Add new comment