How to open the page links on the same screen on the two screen work place?
Hi,
We have 800xA 5.1 FP4 Rev D
In the two screen workplace set up when we open the page links (aspect view) in the second screen the corresponding page opens in the 1st screen (replaces the graphics in the 1st screen) instead of the screen we clicked. The Presentation mode of the links are set to "replace" but it still opens in the other screen. The only way to open the links in the same screen is to click the "set / Clear Primary target".
Is there any way to open the links on the same screen Without pressing the set primary target button?
Could this be because of wrong "profile values" or "View class Values" ?
We have 800xA 5.1 FP4 Rev D
In the two screen workplace set up when we open the page links (aspect view) in the second screen the corresponding page opens in the 1st screen (replaces the graphics in the 1st screen) instead of the screen we clicked. The Presentation mode of the links are set to "replace" but it still opens in the other screen. The only way to open the links in the same screen is to click the "set / Clear Primary target".
Is there any way to open the links on the same screen Without pressing the set primary target button?
Could this be because of wrong "profile values" or "View class Values" ?
Answers
This question has not yet been answered.
by Rajeesh Mariyodan Rank: 40 on 3/29/2020 6:10:18 AM | Like (0) | Report
Did you get any solution to fix this issue ?
Add new comment