Command 'Executing bootstrap on configuration node.': exited with error code -532462766.
Do any one have any idea with the stated error code which I seen during installation of 800xA Server node?
Answers
I met the same problem when installing a new 800xA 6.1 system.
I had wrong windows operative system installed, and the problem got solved buy installing the right one.
I had wrong windows operative system installed, and the problem got solved buy installing the right one.
Add new comment