Undetect Node
Dear Master
I wanna ask, i have project use AS+CS in windows 8.1 as EWS, i use same OS in OWS1 and OWS2 and they can add node, but when i add node HISTORIAN SERVER use OS windows Server 2012 R2 Standart is undetect node. whereas the configure same like OWS.
im use workgroup and domain but not change, node is undetect.
please help me, tankyou for your attention
I wanna ask, i have project use AS+CS in windows 8.1 as EWS, i use same OS in OWS1 and OWS2 and they can add node, but when i add node HISTORIAN SERVER use OS windows Server 2012 R2 Standart is undetect node. whereas the configure same like OWS.
im use workgroup and domain but not change, node is undetect.
please help me, tankyou for your attention
Answers
Hi,
Assumption:800xA V6.x
I am assuming that the SCC is not listing the History server node via the Add Node option (No Green power plug symbol). If this is the case and if the History server node is shown to be reachable in RNRP monitor, then you can manually enter the name of the node when trying to add it.
From experience, the manually entered node name gets listed under the node column and after few seconds the plug icon changes colour from gray to green. The node is then available for deploying functions.

Regards
Rahil
Assumption:800xA V6.x
I am assuming that the SCC is not listing the History server node via the Add Node option (No Green power plug symbol). If this is the case and if the History server node is shown to be reachable in RNRP monitor, then you can manually enter the name of the node when trying to add it.
From experience, the manually entered node name gets listed under the node column and after few seconds the plug icon changes colour from gray to green. The node is then available for deploying functions.
Regards
Rahil
thank you for your information, but how i solve this problem? can you tell me step by step? for more information i attach file
by erik
Which 800xA version do you use?
Add new comment