SM560-S and PM56xx series CPU compatibility
Hi All, Can anyone confirm whether or not the SM560-S can be used with the V3 / PM56xx series CPUs?
I could add the SM560-S to the extension bus on Automation Builder 2.1 but cannot load the project on Automation Builder 2.2.
If I add the PM56xx to a fresh project it will not let me add the safety module to the extension bus.
I could add the SM560-S to the extension bus on Automation Builder 2.1 but cannot load the project on Automation Builder 2.2.
If I add the PM56xx to a fresh project it will not let me add the safety module to the extension bus.
Answers
This question has not yet been answered.
Add new comment