getting error while updating the mcafee patch in 800xa 6.0.3 system

Hi,
i am updating mcafee anti virus DAT file, i am getting an error "
8/6/2019 2:57 PM 800xAInstall ES2 Error: Unable to backup existing file. Not enough rights. : Line: 12 " the dat file was updated today in abb download center. kindly suguest any solution for this. also i am updating the the mcafee version and error details
Answers
I believe contacting the vendor (McAfee) or searching for help on Internet with e.g. Google would be more appropriate...
Have you tried running the task elevated?
Solution This is expected behavior from VSE Patch 9 and later. If the only option is to run the xDAT.exe from a network share, implement the workaround below. Workaround Temporarily or permanently disable the new policy option before performing the DAT update:
Refer KB88263 - New Access Protection rules with VirusScan Enterprise 8.8 Patch 9 and later for more information
- Deselect the new policy option Enable Enhanced Self Protection, located in the Access Protection policy via the ePO console.
- Run the xdat from the network share.
- From the ePO console, enable the AP option Enable Enhanced Self Protection.
Refer KB88263 - New Access Protection rules with VirusScan Enterprise 8.8 Patch 9 and later for more information
by Carsten Jakobsen Rank: 49 on 8/6/2019 4:14:04 AM | Like (0) | Report
You might also want to update VSE 8.8.0 to Patch 13 (8.8.0.2114), i.e. the latest patch approved for use with 800xA
by Harsha.D
have u tried by turning off UAC
Add new comment