i m trying communication between ci854a and ci801, it shows connection down error, help me resolving this
Answers
Hi,
Communication between CI854A and CI801 is done using Profibus DP Check as per the below points
1.Profibus cable termination on both sides.
2.Firmware for CI854 and CI801.
3.Node address setting of CI801.
If u have any error code share the screen shot of it.
Communication between CI854A and CI801 is done using Profibus DP Check as per the below points
1.Profibus cable termination on both sides.
2.Firmware for CI854 and CI801.
3.Node address setting of CI801.
If u have any error code share the screen shot of it.
Do the basic check for cable and Profibus Cable Termination.
Thank you for the detailed problem report. From the details you've provided we are able to tell that the CI854 and the CI801 are not communicating.
For further assistance, you could go though the basic steps of Reading the Manual, checking the base installation details, verifying the connections and address settings, making sure you've used the right purple hose, put the terminators in the right position and then turned it off and on again. All of these suggestions are pure guesswork, much like anything anyone else can tell you from the description provided.
If you think the problem is more than something simple then beg/buy/borrow/steal or otherwise procure the use of one of these things ... https://procentec.com/products/profit...
(BTW, Its almost certainly not the firmware revision of the CI801. Try a new CI801 before worrying about the firmware)
For further assistance, you could go though the basic steps of Reading the Manual, checking the base installation details, verifying the connections and address settings, making sure you've used the right purple hose, put the terminators in the right position and then turned it off and on again. All of these suggestions are pure guesswork, much like anything anyone else can tell you from the description provided.
If you think the problem is more than something simple then beg/buy/borrow/steal or otherwise procure the use of one of these things ... https://procentec.com/products/profit...
(BTW, Its almost certainly not the firmware revision of the CI801. Try a new CI801 before worrying about the firmware)
Add new comment