Graphic Displays Overlapping - 800xA 6.0.3
Hi,
After System 800xA upgrade activities (from 5.1 to 6.03), while navigating through Operator Workplace, the current graphic display shows graphic elements from the graphic display previously displayed. This behavior occurs sometimes (independent of the user, node or graphic display).
I've already checked:
- drivers installed in operator stations;
- hardware issues - all devices are OK;
- memory and CPU usage - OK.
Is there any tip or advice that allows identify possible causes?
Thanks for everyone.
After System 800xA upgrade activities (from 5.1 to 6.03), while navigating through Operator Workplace, the current graphic display shows graphic elements from the graphic display previously displayed. This behavior occurs sometimes (independent of the user, node or graphic display).
I've already checked:
- drivers installed in operator stations;
- hardware issues - all devices are OK;
- memory and CPU usage - OK.
Is there any tip or advice that allows identify possible causes?
Thanks for everyone.
Voted best answer
Hard to tell, could be a MS Windows issue. Please check if "Show Window Contents while Dragging" is disabled. Have a look at other Windows settings that are related to performance an visual behavior.
Add new comment