How to invert Output W.e.r Speed Analog input (4 - 20mA)
hi
i have connected Speed ref to AI i.e 4 - 20mA. How i can configure parameter for increasing speed when Analogue input is 4mA and decrease the speed when Analogue input is 20mA
Drive model ACS355
i have connected Speed ref to AI i.e 4 - 20mA. How i can configure parameter for increasing speed when Analogue input is 4mA and decrease the speed when Analogue input is 20mA
Drive model ACS355
Answers
Hi
I don't have the simulator on hand and so I go from my memory .... try to set parameter 13.01 to 100% and 13.02 to 20% - of course if you use AI1 for reference speed.
Do not forget to set the dip switch for AI1 to current, default setting is for Voltage input
BR
Flavio
I don't have the simulator on hand and so I go from my memory .... try to set parameter 13.01 to 100% and 13.02 to 20% - of course if you use AI1 for reference speed.
Do not forget to set the dip switch for AI1 to current, default setting is for Voltage input
BR
Flavio
Add new comment