New Data-Centre, connection to MOD RTA boards
We moved our external RTA (Mod 300) boards across from our old Data-centre to new ROBO environment.
Most of the VMs were vMotioned across.
We've noticed that the actual speed on the vNIC is 100 MB/half duplex but configured is full duplex.
Also the RNRP analyser is showing a dropoff of 620ms at random times.
We had new cables but reverted to the old crossover cable as a test. Still the same issue.
any ideas?
Most of the VMs were vMotioned across.
We've noticed that the actual speed on the vNIC is 100 MB/half duplex but configured is full duplex.
Also the RNRP analyser is showing a dropoff of 620ms at random times.
We had new cables but reverted to the old crossover cable as a test. Still the same issue.
any ideas?
Answers
Hell Matt,
did you set the NIC Interface on the host for the VM? The ABB Manual ask you to set the speed for the CS itself, but in a virtual environment the host as to be set as well.
We have seen some problems for Intel Dual Network Adpaters. Seeting the Speed on a VM-Host didn't work for them.
BR
Stefan
did you set the NIC Interface on the host for the VM? The ABB Manual ask you to set the speed for the CS itself, but in a virtual environment the host as to be set as well.
We have seen some problems for Intel Dual Network Adpaters. Seeting the Speed on a VM-Host didn't work for them.
BR
Stefan
Add new comment