SattLine alarm stays Auto Blocked in 800xA alarm list
We are working on a phased migration from SattLine to 800xA. One of the techniques we are using is the presentation of SattLine alarms in our 800xA workplace. We have some problems with this solution. When an alarm comes up in SattLine, the alarm also comes up in 800xA. This part is working fine. We can also accept alarms in SattLine and in 800xA.
The only thing that is not working fine is during Auto Blocked. When an alarm in SattLine gets the state Auto Blocked, The alarm in 800xA is also auto blocked. But when the alarm in SattLine returns to normal, the alarm in 800xA remains auto blocked. It should return to normal also in 800xA. Does anyone have any idea what can go wrong?
The only thing that is not working fine is during Auto Blocked. When an alarm in SattLine gets the state Auto Blocked, The alarm in 800xA is also auto blocked. But when the alarm in SattLine returns to normal, the alarm in 800xA remains auto blocked. It should return to normal also in 800xA. Does anyone have any idea what can go wrong?
Answers
This question has not yet been answered.
by TorbenGravesen Rank: 523 on 8/5/2019 1:27:57 PM | Like (0) | Report
Sorry I can't answer your question but I'm very interested in your project. As far as I know there is no ABB product that supports a phased migration from SattLine to 800xA. If you can explain what you actualy are dooing then I may be able to help. Are you using the SattLine OPC server and the OPC AE interface to get the alarms and events from SattLine into 800xA or something else?
What are the other phases and techniques in your project?
Add new comment