How to leave views (faceplates) open during logover in 800xA
Hello,
Normally when a user wants to logover in 800xA he has to close all views (faceplates) before the logover can be done. Is there a way to disable this? Some operators can get really frustrated about this because they have opened a lot of faceplates to follow the process. But when they are not allowed to click a button because of permissions (for some operator actions a higher permission is needed so a 'super' operator has to login) they have close and reopen all of these faceplates.
Normally when a user wants to logover in 800xA he has to close all views (faceplates) before the logover can be done. Is there a way to disable this? Some operators can get really frustrated about this because they have opened a lot of faceplates to follow the process. But when they are not allowed to click a button because of permissions (for some operator actions a higher permission is needed so a 'super' operator has to login) they have close and reopen all of these faceplates.
Answers
But my other question is now, why is this checked by default? Are there some issues with faceplates in combination with logover? Or is this because ate some factories some operators are not allowed to see all faceplates?
I believe overlapping windows ”live their own life” and will not detect if workplace log over.
To ensure all visible graphics and interfaces adhere to the affective user, all overlaps must be closed before logover can take place.
To ensure all visible graphics and interfaces adhere to the affective user, all overlaps must be closed before logover can take place.
See the attachment for the setting. Maybe the buttons in the bottom won't see the log-over, PG2 graphic button can be made to detect the log-over.
Add new comment