xa800
Hi
we have AC800F controller with freelance program . Can we use XA800 program instead of freelance for AC800F controller ? if yes , then how can i do it ? whether if i need to upgrade the firmware of controllers ?
thanks
we have AC800F controller with freelance program . Can we use XA800 program instead of freelance for AC800F controller ? if yes , then how can i do it ? whether if i need to upgrade the firmware of controllers ?
thanks
Voted best answer
But you can put 800xA operations on top of the Freelance Controller.
Answers
You cannot use xA for programming. Programming is only possible from control builder F .
I'm not sure what PCP3.2 is, however you can use 800xA or possibly Compact 800 for your HMI
For 2: If you have Freelance controllers (eg AC800F) then you have to use CBF to create the code. This is not changeable, unless you change your controller. That is AC800M controllers with CBM and AC800F controllers with CBF.
For 2: If you have Freelance controllers (eg AC800F) then you have to use CBF to create the code. This is not changeable, unless you change your controller. That is AC800M controllers with CBM and AC800F controllers with CBF.
PCP is "Process Control Portal".
Add new comment