Freelance Operations 2016 Power options
In Freelance version 2016, the computer's power options, shut down, restart, are not available. How can I make the power options appear?
Answers
Hi,
There is no relation between power button of machine and Freelance Operation; you need to minimize the window by clicking:-
System->Option-> operating system
Regards,
Rachit
There is no relation between power button of machine and Freelance Operation; you need to minimize the window by clicking:-
System->Option-> operating system
Regards,
Rachit
In all Freelance versions, when installed in the production mode, the access to the Windows OS is blocked for safety reasons to prevent the operator from doing other things than operating the process. Access is possible via the menu Tools/System but a password is needed (if configured). The same menu allows you to shut down Freelance Operation, which is good practise before shutting down the PC.
If you use Freelance Operation in a manager's office to view only some KPIs, then you should uncheck the option "Disable the keyboard Windows key" and check the option "disable auto-login" in the Settings, General Settings tab (not sure that those options were already available in Freelance 2016 because I have Freelance 2019 installed) or install Freelance Operations in the Demo mode. Then by pressing the Windows Key you will have acess to the power options and the start button menu.
Either way, also here you should shut down Freelance Operation via the menu Tools/System/Exit Freelance Operation before shutting down the PC. So I don't really see the need for accessing the power options from inside Freelance Operations.
If you use Freelance Operation in a manager's office to view only some KPIs, then you should uncheck the option "Disable the keyboard Windows key" and check the option "disable auto-login" in the Settings, General Settings tab (not sure that those options were already available in Freelance 2016 because I have Freelance 2019 installed) or install Freelance Operations in the Demo mode. Then by pressing the Windows Key you will have acess to the power options and the start button menu.
Either way, also here you should shut down Freelance Operation via the menu Tools/System/Exit Freelance Operation before shutting down the PC. So I don't really see the need for accessing the power options from inside Freelance Operations.
Add new comment