RNRP monitor tool on 800xA operator workplace
One of our customer like to access the RNRP monitor from operator workplace.
Is it possible to call the RNRP monitor from operator workplace ?
Answers
You should be able to display Windows Taskbar and then the RNRP icon is available in the Windows Taskbar notification area (also called the System Tray) at the far right end of the Taskbar. You can open the RNRP status Tool from that icon and then select RnrpMonitor button.
If task bar is required to be hidden then you can access the tool directly from operator screen. create a windows application aspect and point to executable of RNRP tool. Access this windows application aspect from operator graphics.
Add new comment