Ref543, SPA-ZC 400, IEC 61850, configuration in CET
I need to connect my OPC server to REF543 via IEC 61850 protocl. We've bought SPA-ZC 400 Ethernet adapter, now we need to configure it. I installed CET for SPA-ZC 40x v2.2 and use the instruction from ABB site. It says that I need to install connectivity package and enabling it in Connectivity Package Manager, but after installation of connectivity package there is no Connectivity Package Manager on my computer. As I understand without enabling connectivity package I won't be able to import config from CAP505. What I need to do to enable connectivity package?
Link to the instruction I use:
https://search-ext.abb.com/library/Do...
Link to the instruction I use:
https://search-ext.abb.com/library/Do...
Answers
This question has not yet been answered.
Add new comment